Hi community,
I have a question about i.MX6DQ.
I want to know whether i.MX6DQ + BSP support wake-on LAN.
Would you let me know it?
(e.g. L3.10.17_1.0.0-ga : support, kk4.4.2_1.0.0-ga : Not support)
Best Regards,
Satoshi Shimoda
Solved! Go to Solution.
Hi Satoshi
seems it is not supported in official releases,
however one can try attached patch developed internally.
Best regards
igor
Hi Igor,
I was actually looking for this but this patch is for 3.0.35.
there is no fec.h under driver/net/ in the Kernel.
now it has been moved to drivers/net/ethernet/freescale and the patch is implemented for 3.10.31 so far.
I was expecting something in the driver to enable the wake Up to be configurable from the userspace. But I could not see a wakeup to enable
Moreover, the dts does not have any fsl,magic-packet enablement. Only the SoloX is supported.
Hi Rodrigue
Have you fix the wol ?
If you fix the wol, can you share the patch?
Hi Rodrigue
patch was developed at SR-1-1138038028
and you can request internally to develop for 3.10.31
Best regards
igor