Hi Satoshi
seems it is not supported in official releases,
however one can try attached patch developed internally.
Best regards
igor
Hi Igor,
I was actually looking for this but this patch is for 3.0.35.
there is no fec.h under driver/net/ in the Kernel.
now it has been moved to drivers/net/ethernet/freescale and the patch is implemented for 3.10.31 so far.
I was expecting something in the driver to enable the wake Up to be configurable from the userspace. But I could not see a wakeup to enable
Moreover, the dts does not have any fsl,magic-packet enablement. Only the SoloX is supported.