i.MX6DQ support wake-on LAN?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQ support wake-on LAN?

Jump to solution
1,253 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ.

I want to know whether i.MX6DQ + BSP support wake-on LAN.

Would you let me know it?

(e.g. L3.10.17_1.0.0-ga : support, kk4.4.2_1.0.0-ga : Not support)

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (2)
0 Kudos
1 Solution
868 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

seems it is not supported in official releases,

however one can try attached patch developed internally.

Best regards

igor

View solution in original post

0 Kudos
4 Replies
869 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

seems it is not supported in official releases,

however one can try attached patch developed internally.

Best regards

igor

0 Kudos
868 Views
Rodrigue
NXP Employee
NXP Employee

Hi Igor,

I was actually looking for this but this patch is for 3.0.35.

there is no fec.h under driver/net/ in the Kernel.

now it has been moved to drivers/net/ethernet/freescale and the patch is implemented for 3.10.31 so far.

I was expecting something in the driver to enable the wake Up to be configurable from the userspace. But I could not see a wakeup to enable

Moreover, the dts does not have any fsl,magic-packet enablement. Only the SoloX is supported.

868 Views
andyhuang
Contributor I

Hi Rodrigue

Have you fix the wol ?

If you fix the wol, can you share the patch?

0 Kudos
868 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rodrigue

patch was developed at SR-1-1138038028

and you can request internally to develop for 3.10.31

Best regards

igor

0 Kudos