关于 RKS1110

RKS1110
Contributor II
取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
Activity Feed
成員個人資料
Embedded developer being new to SJA1110 and ethernet switch functionality. The NXP SJA1110 is an automotive Ethernet switch with safety capabilities built in, offering integrated 100BASE-T1 PHYs, hardware-assisted security as well as multi-gigabit interfaces. The SJA1110 can be used via SPI from any other microcontroller. Together, this solution provides a flexible and powerful hardware for 2-wire (100BASE-T1) and multi-wire (100BASE-TX) Ethernet. The SJA1110 includes also an ARM Cortex M7 which enables it to do packet inspection or other tasks that use Ethernet or simple GPIO. Looking for more projects to bring in my SJA1110 expertise.
社区统计
发帖数 12
解答 0
给予的奖励 3
赢得的奖励 0
開始會員 ‎08-22-2024
联系我
在线状态
离线
上一次访问的日期
‎11-14-2024 05:20 AM