I have two of these boards. One has stopped showing anything on the serial console and will not boot even using SD cards that work on the good board. I double checked that it is set to boot from SD. I was trying to boot into QNX with a QNX-IFS file that was too large when it became unresponsive and I have not been able to recover since then. Is there a way to recover the bootloader?