RT1176 SEMC Clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 SEMC Clock

Jump to solution
744 Views
chrisgulick
Contributor III

I recently designed an RT1176 system. It uses the SDRAM controller. I can run the example driver app and memory passes read / write tests. I would like to run the memory at 166MHZ. The clocking tree is quite complex and is difficult to get a handle on in short order time. Would someone be able to tell me how to change the memory clock to 166MHZ.

Thank you

0 Kudos
Reply
1 Solution
715 Views
chrisgulick
Contributor III

Jingpan,

Thank you. Went into SEMC clock root and changed SDRAM clock to 166.73MHz.

Memory runs with no errors.

View solution in original post

0 Kudos
Reply
2 Replies
727 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @chrisgulick ,

You can use config tool to configure the clock.

jingpan_0-1671440128905.png

 

Regards,

Jing

 

0 Kudos
Reply
716 Views
chrisgulick
Contributor III

Jingpan,

Thank you. Went into SEMC clock root and changed SDRAM clock to 166.73MHz.

Memory runs with no errors.

0 Kudos
Reply