RT1176 SEMC Clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RT1176 SEMC Clock

跳至解决方案
1,777 次查看
chrisgulick
Contributor III

I recently designed an RT1176 system. It uses the SDRAM controller. I can run the example driver app and memory passes read / write tests. I would like to run the memory at 166MHZ. The clocking tree is quite complex and is difficult to get a handle on in short order time. Would someone be able to tell me how to change the memory clock to 166MHZ.

Thank you

0 项奖励
回复
1 解答
1,748 次查看
chrisgulick
Contributor III

Jingpan,

Thank you. Went into SEMC clock root and changed SDRAM clock to 166.73MHz.

Memory runs with no errors.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,760 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @chrisgulick ,

You can use config tool to configure the clock.

jingpan_0-1671440128905.png

 

Regards,

Jing

 

0 项奖励
回复
1,749 次查看
chrisgulick
Contributor III

Jingpan,

Thank you. Went into SEMC clock root and changed SDRAM clock to 166.73MHz.

Memory runs with no errors.

0 项奖励
回复