RT1176 SEMC Clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,984件の閲覧回数
chrisgulick
Contributor III

I recently designed an RT1176 system. It uses the SDRAM controller. I can run the example driver app and memory passes read / write tests. I would like to run the memory at 166MHZ. The clocking tree is quite complex and is difficult to get a handle on in short order time. Would someone be able to tell me how to change the memory clock to 166MHZ.

Thank you

0 件の賞賛
返信
1 解決策
1,955件の閲覧回数
chrisgulick
Contributor III

Jingpan,

Thank you. Went into SEMC clock root and changed SDRAM clock to 166.73MHz.

Memory runs with no errors.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,967件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @chrisgulick ,

You can use config tool to configure the clock.

jingpan_0-1671440128905.png

 

Regards,

Jing

 

0 件の賞賛
返信
1,956件の閲覧回数
chrisgulick
Contributor III

Jingpan,

Thank you. Went into SEMC clock root and changed SDRAM clock to 166.73MHz.

Memory runs with no errors.

0 件の賞賛
返信