spi interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

spi interface

1,641 Views
amarsoma05
Contributor II

please help us;

we area trying to spi interface  b/w 1176 with 7462 nfc reader , i checked with logic analyzer it will not generating any  signals . help us to how to configure and send data,   

how to change the wakeup mode , the default we press "F8" it will debug, i wants to change spi intrupt to wake up and data to sent and receive in spi only , in this case it prints the data in console we wants to prints the data in terminal how to change it ...

thankyou.......

int main(void) {

uint8_t bCount;
uint16_t status;

phFlashBoot_Main();

/* Initialize LED's */
phLED_Init();

/** Configure IRQ and Data ready ping to LOW on bootup*/
PH_REG_CLEAR_BIT(PCR_PADOUT_REG, PADOUT_IRQ);

/** Configure the Data Ready pin as OUTPUT */
PH_REG_SET_BITN(PCR_PADGPIO1_REG,
PCR_PADGPIO1_REG_GPIO1_EN_OUT_POS);

/** De-Assert the Data Ready pin.*/
PH_REG_CLEAR_BIT(PCR_PADOUT_REG, PADOUT_GPIO1);

/*Configuring GPIO's 4,5,6,7,8 as Inputs*/
for(bCount = 4 ; bCount < 9 ;bCount ++)
{
phhalPcr_ConfigPuPd(bCount,false,true);
phhalPcr_ConfigInput(bCount,true,false,false,false,true,false);
}

PH_HAL_GPIO_SETGPIOVAL(PH_EXHIF_HW_GPIO_IN_PORT_L,0);
PH_HAL_GPIO_SETGPIOVAL(PH_EXHIF_HW_GPIO_IN_PORT_H,1);

PH_HAL_GPIO_SETGPIOVAL(PH_EXHIF_HW_GPIO_COMM_PORT_L,0);
PH_HAL_GPIO_SETGPIOVAL(PH_EXHIF_HW_GPIO_COMM_PORT_M,1);
PH_HAL_GPIO_SETGPIOVAL(PH_EXHIF_HW_GPIO_COMM_PORT_H,0);

/* Create the Event group for HIF transactions */
gphExHif_Hw_HifEvents = phRtos_EventGroupCreate();

/* Execute the Hif Application*/
phExHif_HifTask();
phhalSPIM_Init(PH_HW_SPIM_TIMEOUT) ;
phhalSPIM_Configure(0, 0,E_SPIM_MODE1, 3,0, 0) ;
while(1)
{
status =phhalSPIM_Transmit(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_APPEND_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, 1, cmd_buf, PH_EXHIF_HW_SPIM_CRC_OFFSET);
LOG_X32("sent data status : ",status);
}
/*
status = phhalSPIM_Receive(PH_EXHIF_HW_SPIM_SLAVE, PH_EXHIF_HW_SPIM_INIT_CRC, PH_EXHIF_HW_SPIM_CRC_INIT, 1, dst, PH_EXHIF_HW_SPIM_CRC_OFFSET);
*/

return 0;

}

Tags (1)
0 Kudos
Reply
1 Reply

1,624 Views
FelipeGarcia
NXP Employee
NXP Employee

You can refer to my answer in the following post.

Re: pn7462 interface - NXP Community

Regards,

Felipe

0 Kudos
Reply