Hi,
I have setup the device in Serial Download Programming mode. However, SDP host is still unable to communicate to bootrom of MIMXRT1176
I am receiving following error
# sdphost -u 0x1fc9,0x013d -- error-status
usbhid: received unexpected number of bytes=3fd
getStatusResponse.readPacket error 1.
Status (HAB mode) = 10004 (0x2714) No response from device
Following is my dmesg output:
[ 465.198454] usb 1-1.4.5: new high-speed USB device number 16 using ci_hdrc
[ 465.349953] usb 1-1.4.5: New USB device found, idVendor=1fc9, idProduct=013d, bcdDevice= 0.02
[ 465.350100] usb 1-1.4.5: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 465.350210] usb 1-1.4.5: Product: SE Blank RT Family
[ 465.350289] usb 1-1.4.5: Manufacturer: NXP SEMICONDUCTORS
[ 465.359568] hid-generic 0003:1FC9:013D.000B: hiddev96,hidraw0: USB HID v1.00 Device [NXP SEMICONDUCTORS SE Blank RT Family] on usb-ci_hdrc.1-1.4.5/input0
Solved! Go to Solution.
Hi @razools ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
For the MIMXRT1176, it doesn't need the sdphost, it only uses the blhost, further, I'd highly recommend you to use the GUI tool to contact the MIMXRT1176.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------f
Hi @razools ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
For the MIMXRT1176, it doesn't need the sdphost, it only uses the blhost, further, I'd highly recommend you to use the GUI tool to contact the MIMXRT1176.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------f
Hi @jeremyzhou
The end goal is that I have another imx6 board which will program the MIMXRT1176. To achieve that i needed sdphost. But I figured out from NXP-MCUBootUtility, that for MIMXRT117X the utility uses ble_host (version2.3) to load ivt_flashloader.bin. SDP host isn't used to load flash_loader. I downloaded blhost source code from blhost and now stuck on compiler issue:
Compiling tools/blhost/src/blhost.cpp
../src/blhost.cpp: In member function ‘int BlHost::processOptions()’:
../src/blhost.cpp:851:20: error: ‘LPCUSBSIO_VID’ was not declared in this scope
851 | m_usbVid = LPCUSBSIO_VID;
| ^~~~~~~~~~~~~
../src/blhost.cpp:852:20: error: ‘LPCUSBSIO_PID’ was not declared in this scope
852 | m_usbPid = LPCUSBSIO_PID;
| ^~~~~~~~~~~~~
I am missing blfwk in source of blhost. Can you please suggest me where i can get blfwk package from ?
Hi,
Thanks for your reply.
You can find the source codes of blfwk in the directory(\blhost_2.6.2\src).
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks @jeremyzhou
found it and able to compile it