rt1052 can not detect usb attach or detach

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

rt1052 can not detect usb attach or detach

Jump to solution
1,301 Views
1920844004
Contributor III

As shown below code,my device rt1052 can not detect usb attach or detach,why?

project is: KSDK 2.4.0\boards\evkbimxrt1050\usb_examples\usb_device_hid_generic\bm\mdk

pay attention: #define USB_DEVICE_CONFIG_DETACH_ENABLE   1

USB代码.png

Labels (1)
0 Kudos
Reply
1 Solution
1,168 Views
1920844004
Contributor III

usb_otg_vbus should connect to USB 5V,otherwise can not detect usb attach or detach!

View solution in original post

0 Kudos
Reply
1 Reply
1,169 Views
1920844004
Contributor III

usb_otg_vbus should connect to USB 5V,otherwise can not detect usb attach or detach!

0 Kudos
Reply