pn7462 interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pn7462 interface

1,033 Views
amarsoma05
Contributor II

Hi,

I would like to communicate with SPI between i.mxrt 1176  with pn7462 . how to program there is no example codes for spi in pn7462 .

Is someone have a code example for my request  with the code lines I have to write in my code.

 

Thanks,

 

Tags (1)
0 Kudos
Reply
3 Replies

1,024 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi amar,

We do not have any examples already developed with i.MX RT1170 and PN7462. However, we have several SPI examples and drivers for i.MX RT1170 in our MCUXpresso SDK that can help you with this task. You can download it from the following link.

Welcome | MCUXpresso SDK Builder

Best regards,

Felipe

0 Kudos
Reply

1,016 Views
amarsoma05
Contributor II
Spoiler
 Sip interface

I need spi interface for pn7462 NFC reader example...  if any is there ......share the link...

 

Tags (1)
0 Kudos
Reply

1,001 Views
FelipeGarcia
NXP Employee
NXP Employee

You will need NFC reader library, you can get it from this link. As I mentioned, we do not have this library ported to the RT1170. However, we do have a porting guide for i.MX RT1050, you could take it as reference as do something similar with PN7462.

NFC Reader Library Porting to i.MX RT1050 - NXP Community

Best regards,

Felipe

0 Kudos
Reply