pn7462 interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

pn7462 interface

976 次查看
amarsoma05
Contributor II

Hi,

I would like to communicate with SPI between i.mxrt 1176  with pn7462 . how to program there is no example codes for spi in pn7462 .

Is someone have a code example for my request  with the code lines I have to write in my code.

 

Thanks,

 

标记 (1)
0 项奖励
回复
3 回复数

967 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi amar,

We do not have any examples already developed with i.MX RT1170 and PN7462. However, we have several SPI examples and drivers for i.MX RT1170 in our MCUXpresso SDK that can help you with this task. You can download it from the following link.

Welcome | MCUXpresso SDK Builder

Best regards,

Felipe

0 项奖励
回复

959 次查看
amarsoma05
Contributor II
破坏者
 Sip interface

I need spi interface for pn7462 NFC reader example...  if any is there ......share the link...

 

标记 (1)
0 项奖励
回复

944 次查看
FelipeGarcia
NXP Employee
NXP Employee

You will need NFC reader library, you can get it from this link. As I mentioned, we do not have this library ported to the RT1170. However, we do have a porting guide for i.MX RT1050, you could take it as reference as do something similar with PN7462.

NFC Reader Library Porting to i.MX RT1050 - NXP Community

Best regards,

Felipe

0 项奖励
回复