lwip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lwip

1,180 Views
Mit_3000GT_VR4
Contributor II

Hi,

I looking at the lwip examples in the SDK for the i.MXRT1021, I could only find flexspi_nor_sdram_debug and flexspi_nor_sdram_release.  On my board, I don’t have any SDRAM.  Is there a reason for these examples not to have flexspi_nor_debug or flexspi_nor_release?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,176 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there a reason for these examples not to have flexspi_nor_debug or flexspi_nor_release?
-- Please go to download the updated SDK library, it provides the flexspi_nor_debug and flexspi_nor_release options.

jeremyzhou_1-1635500257589.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply