Hello
on the 105x
trying to use lpspi interface to initiate spi transactions
I am using the SDK example: lpspi_btb_interrupt_master
I am connected to an external board with the flash
trying to read the JEDEC ID with opcode 0x9F according to windbond spec:
but I dont receive any data on the MISO line:
or with the lpspi poliing example:
when using the FLEX_SPI interface, with SDK example "nor_polling_transfer" ,no problems:
what could be the issue?
maybe these examples lpspi_btb_interrupt_master and lpspi_btb_polling_master are not fit to this kind of task? maybe they are BTB dedicated?
thanks
已解决! 转到解答。
the issue was some hardware issues
example reading jedec code:
/*Master config*/
LPSPI_MasterGetDefaultConfig(&masterConfig);
masterConfig.baudRate = TRANSFER_BAUDRATE;
masterConfig.whichPcs = EXAMPLE_LPSPI_MASTER_PCS_FOR_INIT;
srcClock_Hz = LPSPI_MASTER_CLK_FREQ;
LPSPI_MasterInit(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterConfig, srcClock_Hz);
uint32_t jedecId;
uint8_t readdata;
PRINTF("READ JEDEC");
jedecId = 0;
masterTxData[0] = 0x9F;
masterTxData[1] = 0xFF;
masterTxData[2] = 0xFF;
masterTxData[3] = 0xFF;
masterTxData[4] = 0xFF;
/*Start master transfer, transfer data to slave.*/
masterXfer.txData = masterTxData;
masterXfer.rxData = &jedecId;
masterXfer.dataSize = 4;
masterXfer.configFlags =
EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;
LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);
example for reading and programming page in 4 byte mode (32 bit address, after sending 0xB7 opcode):
PRINTF("READ ADDRESS 0X0");
uint8_t page[262];
masterTxData[0] = 0x0B;
masterTxData[1] = 0x0;
masterTxData[2] = 0x0;
masterTxData[3] = 0x0;
masterTxData[4] = 0x0;
masterTxData[5] = 0xFF; //DUMMY BYTE
/*Start master transfer, transfer data to slave.*/
masterXfer.txData = masterTxData;
masterXfer.rxData = page;
masterXfer.dataSize = 262;
masterXfer.configFlags =
EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;
LPSPI_SetDummyData(EXAMPLE_LPSPI_MASTER_BASEADDR, 0xFF); // Set dummy data to 0xFF
LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);
PRINTF("WR EN");
masterTxData[0] = 0x06;
/*Start master transfer, transfer data to slave.*/
masterXfer.txData = masterTxData;
masterXfer.rxData = NULL;
masterXfer.dataSize = 1;
masterXfer.configFlags =
EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;
LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);
PRINTF("PROGRAM ADDRESS 0X0");
uint8_t progpage[267];
int i;
for( i=5;i<267;i++)
{
progpage[i] = i - 5;
}
progpage[0] = 0x02;
progpage[1] = 0x0;
progpage[2] = 0x0;
progpage[3] = 0x0;
progpage[4] = 0x0;
/*Start master transfer, transfer data to slave.*/
masterXfer.txData = progpage;
masterXfer.rxData = NULL;
masterXfer.dataSize = 262;
masterXfer.configFlags =
EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;
LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);
the issue was some hardware issues
example reading jedec code:
/*Master config*/
LPSPI_MasterGetDefaultConfig(&masterConfig);
masterConfig.baudRate = TRANSFER_BAUDRATE;
masterConfig.whichPcs = EXAMPLE_LPSPI_MASTER_PCS_FOR_INIT;
srcClock_Hz = LPSPI_MASTER_CLK_FREQ;
LPSPI_MasterInit(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterConfig, srcClock_Hz);
uint32_t jedecId;
uint8_t readdata;
PRINTF("READ JEDEC");
jedecId = 0;
masterTxData[0] = 0x9F;
masterTxData[1] = 0xFF;
masterTxData[2] = 0xFF;
masterTxData[3] = 0xFF;
masterTxData[4] = 0xFF;
/*Start master transfer, transfer data to slave.*/
masterXfer.txData = masterTxData;
masterXfer.rxData = &jedecId;
masterXfer.dataSize = 4;
masterXfer.configFlags =
EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;
LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);
example for reading and programming page in 4 byte mode (32 bit address, after sending 0xB7 opcode):
PRINTF("READ ADDRESS 0X0");
uint8_t page[262];
masterTxData[0] = 0x0B;
masterTxData[1] = 0x0;
masterTxData[2] = 0x0;
masterTxData[3] = 0x0;
masterTxData[4] = 0x0;
masterTxData[5] = 0xFF; //DUMMY BYTE
/*Start master transfer, transfer data to slave.*/
masterXfer.txData = masterTxData;
masterXfer.rxData = page;
masterXfer.dataSize = 262;
masterXfer.configFlags =
EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;
LPSPI_SetDummyData(EXAMPLE_LPSPI_MASTER_BASEADDR, 0xFF); // Set dummy data to 0xFF
LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);
PRINTF("WR EN");
masterTxData[0] = 0x06;
/*Start master transfer, transfer data to slave.*/
masterXfer.txData = masterTxData;
masterXfer.rxData = NULL;
masterXfer.dataSize = 1;
masterXfer.configFlags =
EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;
LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);
PRINTF("PROGRAM ADDRESS 0X0");
uint8_t progpage[267];
int i;
for( i=5;i<267;i++)
{
progpage[i] = i - 5;
}
progpage[0] = 0x02;
progpage[1] = 0x0;
progpage[2] = 0x0;
progpage[3] = 0x0;
progpage[4] = 0x0;
/*Start master transfer, transfer data to slave.*/
masterXfer.txData = progpage;
masterXfer.rxData = NULL;
masterXfer.dataSize = 262;
masterXfer.configFlags =
EXAMPLE_LPSPI_MASTER_PCS_FOR_TRANSFER | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;
LPSPI_MasterTransferBlocking(EXAMPLE_LPSPI_MASTER_BASEADDR, &masterXfer);
Hi @adi2Intel,
The LPSPI and FlexSPI modules are inheritably different. As stated by my colleague on the following community post: "the FlexSPI module is dedicated to communicate with Flash-like serial devices. It has a set of dedicated features (like LUT command sequences) for such type of accesses. For SPI communication with a "generic" (non-Flash) SPI devices, the LPSPI module should be used."
As you mention, the BTB examples are meant to show a generic SPI communication between two boards. If you are looking for a standard SPI communication example (not between two boards) refer to the "lpspi_interrupt" example.
BR,
Edwin.
Can we use the LPSPI to read and write a flash device device using single SPI protocol?
or even use the LPSPI to read JEDEC ID?
basically our device using the flexSPI port to read and write another flash device , and our device has 4 LPSPI ports .
Hi @adi2Intel,
From the W25Q32JV Datasheet: "The W25Q32JV supports the standard Serial Peripheral Interface (SPI)", so it is possible. As mentioned on your previous post, a good example to refer to for LPSPI read/write with NOR Flash would be the "flashloader" example under "bootloader_examples". With the right modifications to the LUT table, you should be able to communicate with the NOR Flash without issues.
BR
Edwin.