Hi!
Configuration Descriptor in example has the following values:
number of bytes occupied by one audio subslot - 2
number of effectively used bits from the available bits in an audio subslot - 16
Any other values not work.(for example: bSubslotSize=2 bBitResolution=8;)
There are no error messages during initialization (win10),
but playback is not going on. Some players report: "Unrecoverable playback error: Unsupported stream".
I have studied the UAC2.0 standard, but I have not found other places where it is necessary to specify the bit depth of the samples.
Can someone help me ?
Hi @SergioNpl ,
Which SDK version you are using? So far the latest supports RT1010 is ver 2.14.0 , but I could not find something like bBitResolution in the latest version. Please kindly clarify.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------