iMX RT1064 can use ethernet without phy? phy-less or MAC-to-MAC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX RT1064 can use ethernet without phy? phy-less or MAC-to-MAC

1,269 Views
jh_cheon
Contributor I

I'm trying to build system with using iMX RT1064.

and there's need switch ic which is support both RMII MAC mode and RMII PHY mode.

I couldn't find any evidence that RT1064 can use RMII connection between ethernet switch without phy.

Is it possible to use RT1064 with phy-less and also includes PTP?

or do i have to use PHY? 

I attached the simple block diagram.

 

Thanks.

 

 

0 Kudos
Reply
1 Reply

1,255 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi  jh_cheon,

    RT1064 chip don't have the on chip PHY,  if you want to release the ethernet communication, you still need to add the external PHY chip.

   I suggest you refer to the MIMXRT1064-EVK board, add the external PHY to release two board's ethernet  communication.

 

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards.

Kerry

0 Kudos
Reply