Hi,
I would like to use the LPUART of the EVK board to receive messages of unknown size.
For this purpose, I would like to combine the usage of idle line interrupt and the eDMA mechanism.
The examples found in the SDK are with IRQ separately and eDMA separately, how can I combine the two?
Is there a relevant example code?
Thanks,
Ira.
已解决! 转到解答。
Hello
You can use the example "lpuart_edma_rb_transfer" from the RT10xx SDKs as a reference for Idle Line Detection.
If you have more questions do not hesitate to ask me.
Best regards,
Omar
Hello
You can use the example "lpuart_edma_rb_transfer" from the RT10xx SDKs as a reference for Idle Line Detection.
If you have more questions do not hesitate to ask me.
Best regards,
Omar