i.MXRT1170-EVK LPUART idle line interrupt with EDMA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MXRT1170-EVK LPUART idle line interrupt with EDMA

ソリューションへジャンプ
1,212件の閲覧回数
igrinberg
Contributor II

Hi,

I would like to use the LPUART of the EVK board to receive messages of unknown size.

For this purpose, I would like to combine the usage of idle line interrupt and the eDMA mechanism.

The examples found in the SDK are with IRQ separately and eDMA separately, how can I combine the two?

Is there a relevant example code?

Thanks,
Ira.

 

0 件の賞賛
返信
1 解決策
1,194件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

You can use the example "lpuart_edma_rb_transfer" from the RT10xx SDKs as a reference for Idle Line Detection.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,195件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

You can use the example "lpuart_edma_rb_transfer" from the RT10xx SDKs as a reference for Idle Line Detection.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 件の賞賛
返信