Can the RT1170 support a MIPI display at 1080x1920 resolution at 60Hz ?
I believe through some research, the RT1170 cannot support this resolution at 60 Hz, but can we confirm it can support this resolution at 30 Hz? I'm having troubles getting a display to work, thus the questioning...
Hello
I hope you are well.
RT1170 Supports up to WXGA(1366x768)@60fps with rich UI & application. If the memory supports it then we could decrease the fps so the resolution is higher.
Best regards,
Omar