i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled

Jump to solution
1,381 Views
SeenFan
Contributor II

Trying to enable SSC on RT1170 EVK with MCUXpresso.

Ref: AN12879

Steps:

1. Base project: SDK Example evkmimxrt1170_semc_cm7

2. Using IDE to config SSC 

IDE_Clocking.png

source_diff.png

3. Boot failed

Boot_Failed.png

4. Sometimes can boot normally (~ 1/50)

Any step I missed?

Regards

Seen

0 Kudos
Reply
1 Solution
1,320 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @SeenFan ,

This is because RT1170 FlexSPI use PLL2 as clock source when use default configure. When you change PLL2 frequency, FlexSPI may fail to get next instruction. To resolve this, you can put fsl_clock.c to SRAM. Please refer to my demo code.

 

Regards,

Jing

View solution in original post

0 Kudos
Reply
4 Replies
1,321 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @SeenFan ,

This is because RT1170 FlexSPI use PLL2 as clock source when use default configure. When you change PLL2 frequency, FlexSPI may fail to get next instruction. To resolve this, you can put fsl_clock.c to SRAM. Please refer to my demo code.

 

Regards,

Jing

0 Kudos
Reply
1,295 Views
SeenFan
Contributor II

Hi Jin,

If I want to locate and run program on SDRAM. 
What I need to pay attention to?

 

Regards

Seen

0 Kudos
Reply
1,287 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @SeenFan ,

SDRAM can be initialized by DCD and boot ROM.  Then boot ROM will copy your application code to SDRAM. I think the most important thing is the cache problem. You can refer to these link.

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-move-CM4-core-project-to-SDRAM-in-RT1176...
2.debug in sdram
https://community.nxp.com/t5/MCUXpresso-IDE/Running-and-debugging-program-in-SDRAM/m-p/1405167
3.Using NonCached Memory on i.MXRT
https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-NonCached-Memory-on-i-MXRT/ta-p/1183369

Regards,

Jing

 

0 Kudos
Reply
1,302 Views
SeenFan
Contributor II

Hi Jing,

It works. Thanks a lot.

 

Regards

Seen

0 Kudos
Reply