Dear NXP,
Would be awesome if you could add .dts output (and even kconfig) to the Pins tool for the i.MX RT series.
This is very useful when designing with RT's using the Zephyr project RTOS.
Thanks
Hello,
Thanks for your feedback! I will pass the information to the corresponding team.
Have a great day,
Victor
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------