dsp_mu_polling not functioning properly

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

dsp_mu_polling not functioning properly

跳至解决方案
3,762 次查看
Hthornburgh
Contributor III

I've got the RT685-AUD-EVK and have been using it successfully until recently. MCUXpresso seems to indicate that things are being built and flashed properly however I'm not getting the expected outcome from the board. I attempted running hello_world and dsp_mu_polling to check and see if at least those would function, but I am not getting anything printed to the terminal. Unsure of what I may have done to cause this, but is there any way I can return in to a zero state and follow the getting started instructions again?

标签 (1)
0 项奖励
回复
1 解答
3,732 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @Hthornburgh ,

You can download a CM33 project which can initialize DSP core first.

 

Regards,

Jing

在原帖中查看解决方案

5 回复数
3,753 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @Hthornburgh ,

There isn't zero state or you can erase the flash. Can you please check all the switchs and jumpers on the board. You can take the photo of RT685-AUD-EVK in the Getting_Start document as example.

 

Regards,

Jing

0 项奖励
回复
3,743 次查看
Hthornburgh
Contributor III

I'm thinking maybe the issue is that when I try to execute command "xt-ocd.exe -c topology.xml" I get this response here. Any suggestions of what to try to get this to work properly?

Xtensa cmd error.png

 

0 项奖励
回复
3,733 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @Hthornburgh ,

You can download a CM33 project which can initialize DSP core first.

 

Regards,

Jing

3,730 次查看
Hthornburgh
Contributor III

Any suggestions on a project that would work? I tried hello world and still was having the same issues after running

0 项奖励
回复
3,736 次查看
Hthornburgh
Contributor III

I also receive this error in xtensa when trying to debug

Hthornburgh_0-1668727446981.png

 

 

 

0 项奖励
回复