Why no any IMX series product supporting PDM audio microphone?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why no any IMX series product supporting PDM audio microphone?

1,726 Views
mayqueen
Contributor IV

My target Platform is IMX7 and IMXRT1050, both adapted Buildroot, it works very well but audio function is always failed using PDM microphone, it seems very strange when I search no any post or project, it's a good cost down way but why no anyone to do it?

 

I adapted simple-audio-card driver as following setting:

 

    sound {
        compatible = "simple-audio-card";
        simple-audio-card,name = "OnboardIM69D130";
        simple-audio-card,format = "pdm";
        simple-audio-card,bitclock-master = <&cpu_dai>;
        simple-audio-card,frame-master = <&cpu_dai>;
        simple-audio-card,widgets =
            "Microphone", "Mic Jack";
        simple-audio-card,routing =
            "MIC_IN", "Mic Jack";

 

        cpu_dai: simple-audio-card,cpu {
            sound-dai = <&sai1>;
            system-clock-frequency = <2400000>;
            dai-tdm-slot-num = <1>;
            dai-tdm-slot-width = <16>;
        };

 

        simple-audio-card,codec {
            sound-dai = <&dummy_codec>;
        };
    };

 

 

and dmesg has no error but also no generate any ALSA devices, please someone can give me directions, thanks!

Wig

0 Kudos
Reply
1 Reply

1,319 Views
igorpadykov
NXP Employee
NXP Employee

Hi May

i.MX8M Mini supports pdm

pastedImage_2.jpg

software description can be found on

i.MX Software|NXP 

fsl-imx8mq-evk-pdm.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

imx-pdm.c\fsl\soc\sound - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply