Unable to run example on MIMXRT1170 EVKB Core M7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to run example on MIMXRT1170 EVKB Core M7

ソリューションへジャンプ
556件の閲覧回数
jayesh_joshi
Contributor IV

Hi 

 

I am trying to run the "mpp_camera_ultraface_view_tflm_cm7" example on the recently purchased MIMRT1170 EVKB. The results are the same for all other examples, which have "cm7" at the end.

No jumper changes on the MIMRT1170 EVKB. Image attached for reference.

 

jayesh_joshi_0-1710417792823.jpeg

 

The building and flashing steps are as below:. Is there something missing in the steps I am following? I have gone through the user guide but nothing pops out.  I am using onboard debugger for debugging. 

jayesh_joshi_1-1710417792744.png

 

 

jayesh_joshi_2-1710417792825.png

 

jayesh_joshi_3-1710417792822.png

 

 

タグ(2)
0 件の賞賛
返信
1 解決策
529件の閲覧回数
jayesh_joshi
Contributor IV

@EdwinHz 

Thank you for the reply.

 

Getting started guide took me to SDK of MIMXRT1170-EVK instead of MIMXRT1170-EVKB. That was the issue with example not running.

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
530件の閲覧回数
jayesh_joshi
Contributor IV

@EdwinHz 

Thank you for the reply.

 

Getting started guide took me to SDK of MIMXRT1170-EVK instead of MIMXRT1170-EVKB. That was the issue with example not running.

 

0 件の賞賛
返信
535件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @jayesh_joshi,

Do you see this issue with other example codes from the SDK? Or only with this one?

I noticed that MCUXpresso only imports 1 readme file, but the example seems to have 2. On the example location from the SDK installation path, you will find one readme on the main example folder and another on a subfolder called "doc".

EdwinHz_0-1710445257561.png

Here's the example location: 

"C:\Users\<user>\mcuxpresso\02\SDKPackages\SDK_2_15_000_MIMXRT1170-EVKB.zip\boards\evkbmimxrt1170\eiq_examples\mpp_camera_ultraface_view_tflm"

MCUXpresso seems to load the one under the "doc" folder, but make sure to follow both.

BR,
Edwin.

0 件の賞賛
返信