USB to CAN-FD bridge?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB to CAN-FD bridge?

815 Views
dav1
Contributor V

Hi,

Are there any existing implementaions for making a USB to CAN FD adapter on the RT series?

 

...preferably paired with, or compatible with a good host-side lib in python or similar
(not familiar at all if there is a "go to" host solution to interact with CAN-FD bridges via usb/libusb, anyone with insights?) [linux only is fine here]

Labels (2)
0 Kudos
Reply
1 Reply

800 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @dav1,

Unfortunately, there isn't an example that matches all the requirements but in the SDK there are examples that show how to work with the CAN and multiple USB classes that could help you with your application.

Best Regards,
Alexis Andalon

0 Kudos
Reply