Hi All,
We are experiencing an issue with the TRNG. Inside the driver, there is mention of a defect in function trng_ReadEntropy().
/* Dummy read. Defect workaround. * TRNG could not clear ENT_VAL flag automatically, application * had to do a dummy reading operation for anyone TRNG register * to clear it firstly, then to read the RTENT0 to RTENT15 again */
We are finding that after 1 or more reads, the peripheral starts to behave inconsistently, and cannot be used.
Is the Errata documented anywhere?, does it apply to the iMXRT1021?
Thanks,
Chris.
Hi Chris,
there is a TRNG example in SDK. Have you tried it? It read 10 RNG data continuously. It hasn't any problem.
Regards,
Jing
Hi,
We found the default Frequency Count Limit was too low, so it was tripping its own error detection.
So it is resolved now.
Regards,
Chris.
Hi Chris,
May I please ask what you changed the Frequency Count Limit to? The default range in fsl_trng.c seems to be:
#define TRNG_USER_CONFIG_DEFAULT_FREQUENCY_MAXIMUM 25600
#define TRNG_USER_CONFIG_DEFAULT_FREQUENCY_MINIMUM 1600
Thanks, Nick