I am trying to do a cold reset on the I.MXRT1015 EVK. I am running the example code src_reset_source and I always get a reset source value of 0x1 (ipp_reset_b). I am trying to generate a ipp_user_reset_b using SW2 which should be connected to ONOFF, but this button does nothing.
Hi Chris K
If you want to get the cold reset, please check the Figure 20-5. SRC inputs and outputs in the RT1015 reference manual.
When you use the SRC_ONOFF, do you check the SRC_SRSR[ipp_user_reset_b], whether this bit is set or not?
Wish it helps you!
If you still have questions about it, please kindly let me know.
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------