SRAM and SDRAM config by MCUXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRAM and SDRAM config by MCUXpresso

Jump to solution
711 Views
Eugene3
Contributor II

I'm designing an i.MXRT1170 application board. It has SRAM and SDRAM on the SEMC bus.

I'm trying to configure SRAM and SDRAM setting by MCUXpresso IDE but an error occurred.

How can I configure both of SRAM and SDRAM at the same application by MCUXpresso IDE? 

 

[What I've done]

I added SEMC(for SRAM) and SEMC_2(for SDRAM) from Register initialization section in Peripherals. Then an error has occurred like the following.

"Peripherals: SEMC used in multiple component instances : SEMC"

 

 

0 Kudos
Reply
1 Solution
679 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Config tools allow you to create the init parameters for SEMC device however there is a limitation that it only creates the parameters for one device.
So you need to write manually the parameters and initialization for the other device.

Best regards,
Omar

View solution in original post

0 Kudos
Reply
2 Replies
674 Views
Eugene3
Contributor II

Hi @Omar_Anguiano 

Thank you for your information. I'll write manually for other devices.

0 Kudos
Reply
680 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Config tools allow you to create the init parameters for SEMC device however there is a limitation that it only creates the parameters for one device.
So you need to write manually the parameters and initialization for the other device.

Best regards,
Omar

0 Kudos
Reply