SEMC Serial NAND

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SEMC Serial NAND

1,181件の閲覧回数
Ankush_9881
Contributor II

Hello All,

 I am working with iMXRT1176, I have one query like, Is it possible to interface Serial SLC NAND flash via SEMC1 and boot the MCU ?

Also with above configuration , is it possible to use SDRAM and SLC NAND Flash on SEMC ?

(example: NAND Flash MX35LFxGE4AB) 

0 件の賞賛
返信
2 返答(返信)

757件の閲覧回数
maouncle
Contributor I

Can you recommand one type nand device for iMXRT1176?

0 件の賞賛
返信

1,160件の閲覧回数
jay_heng
NXP Employee
NXP Employee

SEMC can only work with Raw NAND (ONFI 1.0), you can use FlexSPI to interface Serial (SPI) NAND (JESD216).

it is possible to use SDRAM and Raw NAND Flash on SEMC

0 件の賞賛
返信