SDIO fail on Murata wifi module(IW416) and RT1062

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDIO fail on Murata wifi module(IW416) and RT1062

1,794 Views
antoniohsu888
Contributor II

Our PCBAs use a RT1062 to control murata LBEE5CJ1XK IW416 wifi module.

As I check the SDK 2.11.0 already include murata patch for wifi module.

My SDK version is 2.11.1.

[1] Project example: wifi_cli

[2] In app_config.h , I configure the murata settings.

[3]Interface voltage 3.3v

and control the muratu 1xk PMIC_EN to enable the wifi power.

#elif defined(WIFI_IW416_BOARD_MURATA_1XK_USD)
#define WIFI_BT_TX_PWR_LIMITS "wlan_txpwrlimit_cfg_murata_1XK_WW.h"
#define SD8978
#define SDMMCHOST_OPERATION_VOLTAGE_3V3
#define SD_TIMING_MAX kSD_TimingDDR50Mode
#define WIFI_BT_USE_USD_INTERFACE
#define WLAN_ED_MAC_CTRL

[4]Test the project, the code lock on 

sdio_init() ->sdio_drv_init() ->sdio_card_init() ->SDIO_CardInit()->sdiocard_init()->SDIO_ProbeBusVoltage() ->SDIO_SendOperationCondition() (Get IO OCR-CMD5 with arg0 )

Strange thing is only SDIO_GoIdle() pass,

the SDIO_GoIdle() also use SDMMCHOST_TransferFunction() to send command via SDIO to wifi chip.

And the next command SDIO_SendOperationCondition() (Get IO OCR-CMD5 with arg0 ) is failed.

I can measure the SDIO clock and cmd signals.

 

Any idea for what may be the problem ?

Thank you.

 

0 Kudos
Reply
4 Replies

1,780 Views
antoniohsu888
Contributor II

The murata wifi module seems not active.

so the go idle command return OK, because it does not need return code.

But other command which need return code will fail.

By the way, do you see this kind of fail for Murata wifi 1xk module connected with RT1062 ? 

0 Kudos
Reply

1,769 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me trying the SDK version 2.12?

 

Regards,

Estephania

0 Kudos
Reply

1,763 Views
antoniohsu888
Contributor II

Hi,  Estephania:

OK, I will try it.

And I find may be the murata module is not active.

I had used the same project (wifi_cli 2.11.1) with the AW wifi module on RT1060 EVKB.

It can work,so I think the SDIO and wifi driver is no problem.

Now I try to purchase a Murata 1xk wifi EVK to test with RT1060 EVKB first.

At the same time, would you please check the SDIO command signal for go_idle commnad.

Go_idle do not need return code, so it only on send command.

But other command which need return code is failed.

On the SDIO clock, does the extra clock after the CRC is normal or abnormal ?

Thank you.

BR. Antonio.

Tags (1)
0 Kudos
Reply

1,743 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

In the SDk documentation you can find several documents, between them there is the UM11443-NXP-Wi-Fi-and-Bluetooth-Debug-Feature-Configuration-Guide-for-i.MX-RT-Platforms .

You can try to enable the

 

CONFIG_WIFI_SDIO_DEBUG

CONFIG_WIFI_IO_DEBUG

CONFIG_WIFI_CMD_RESP_DEBUG

 

With this it might be easier to validate in which part the program is getting stuck

 

regards

 

0 Kudos
Reply