RT1064: Problems with board bring up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1064: Problems with board bring up

Jump to solution
2,013 Views
MSchulz
Contributor II

Hello NXP,

I made a custom board with an RT1064 and I am now in the bring-up phase.

After applying and proofing all the voltages and power-on sequences I tried to connect to the chip via "MCU-Link Pro" in J-Link mode and with "MCU-Boot-Utility".

For the use of the "MCU-Boot-Utility" I applied the "Serial Downloader" mode by setting the boot_mode[1:0] bits to "01".

Both methods failed - I just cant connect to the device.

The device gets quite warm (appr. 60°C) and does nothing. (Connections of the Power Pins already double-checked)

I have no glue how to approach this problem.

So it would be nice, if someone could explain, what is crucial to bring the RT1064 into operation.

Many thanks in advance and best regards,

Marco Schulz.

 

0 Kudos
Reply
1 Solution
1,887 Views
MSchulz
Contributor II

Done!

The solution was the wrong usage of the NVCC_PLL pin!

Not to forget: as the PLL is in the 1.1V domain, the output amplitude of an external clock source in bypass mode which drives the PLL (connected to XTALI) must also not exeed 1.1V!

Now my board is brought up and I can start developing software

View solution in original post

8 Replies
1,877 Views
davenadler
Senior Contributor I

Congratulations! Hope you don't find as many problems with FSL drivers as I have ;-(

0 Kudos
Reply
1,888 Views
MSchulz
Contributor II

Done!

The solution was the wrong usage of the NVCC_PLL pin!

Not to forget: as the PLL is in the 1.1V domain, the output amplitude of an external clock source in bypass mode which drives the PLL (connected to XTALI) must also not exeed 1.1V!

Now my board is brought up and I can start developing software

1,993 Views
davenadler
Senior Contributor I

@MSchulzwrote: The device gets quite warm (appr. 60°C) and does nothing.

That certainly should not happen - something is seriously wrong!
I hope you have not made the same mistake I did and crossed up 1.1v supply (output and input to CPU) and 3.3v net. Do double-check the 1.1v net. For your sake I hope this is the wrong answer!

Otherwise, use an IR thermometer gun (well, or IR camera, or your finger) to find out what else is hot on your board.

Best Regards, Dave

0 Kudos
Reply
1,959 Views
MSchulz
Contributor II

Hi Dave,

thanks for your reply.

What did you mean with crossed 1.1V and 3.3V net? Did you connect 3.3V to the VDD_SOC pins?

I added my schematic page for the RT1064 power supply:

MSchulz_0-1683527580734.png

I think, I made the core-supply the same like shown in the "Hardware Development Guide for the MIMXRT1050/MIMXRT1060 Processor" on page 7:

MSchulz_1-1683527756217.png

The measured voltage at DCDC_SENSE/VDD_SOC_IN is 1.15V which is in the typical range shown in table 1 of the before mentioned guide.

All 3.3V-voltages are in the range of 3.27V to 3.29V.

Do you have any other suggestions?

Best regards,

Marco.

 

 

0 Kudos
Reply
1,956 Views
MSchulz
Contributor II

SORRY, I think I found my mistake!

I feed 3.3V into the pin "NVCC_PLL" which is obviously ment to be a cap-bypass pin for the internal PLL supply.

**bleep** happens...

0 Kudos
Reply
1,947 Views
davenadler
Senior Contributor I

Glad you found the problem!
At least this one, you can solder down a new RT with the pin bent up and fly-wire the PLL cap.
Then you can find the next bug before respinning the board
Good luck!
Best Regards, Dave

0 Kudos
Reply
1,944 Views
MSchulz
Contributor II

yes, its not that easy because the RT is a BGA but we are lucky that the wrong connection is right at the edge of the package. so we can de-solder the old one cut the fanout to 3.3V and try to apply a thin wire to connect to a cap before we solder a new RT in again...

0 Kudos
Reply
1,940 Views
davenadler
Senior Contributor I

Sorry I forgot about BGA, I'm using RT1024 in easier package.
But, that RT is probably toast if it got that hot.
Good luck!

0 Kudos
Reply