Hi,
We are building an application card based on i.MX 1050, about the SEMC interface, I saw it support SRAM in Chapter 49, but when I veiw the Signal, I can't see the pin of RD and WR. The pin of SEMC_WE, the description is like this "Write Enable (For SDRAM only)" which make me confused.I can't find other RD and WR singal to support the SRAM like IS62WV25616BLL-55TLI-TR.
And I also can't find it on Pins Tool for i.MX.
So, I wanted know if,
1. My understanding is correct with respect to parallel bus interface.
2. Is there any another way I can make it?
Thanks,
Zefeng Tao
Hi Taoze Feng,
But IS62WV25616BLL also hasn't RD and WR. Most current commercial SRAM hasn't these pins.
MCUXpresso IDE has integrated pin config tool. If you use Keil/IAR, you can use MCUxpresso Config Tools to configure pins. It can be downloaded from
Regards,
Jing
Hi, Jing
Thanks for your reply, we always used the IC like LY62256SL which had OE and WE.and now we want to use I.MX RT1050,and now I didn't know how to design to achieve this with parallel bus interface, so we now commucate with the IC using serial interface like spi.
But I also want to know how to use the parallel interface, It means I should use the IC like the IS62WV25616BLL which without RD and WR,and I must match the sequence if I use the FPGA. Is it means I.MX RT1050 can't support the IC like LY62256SL. Sorry, I don't konw how the upload the pic.
Now I had use the MCUxpresso Config Tools to configure pins and the keil to compile th project,thanks.