Parallel Bus Interface (SRAM kind of) in i.MX 1050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Parallel Bus Interface (SRAM kind of) in i.MX 1050

900 Views
TaoZefeng
Contributor I

Hi,

     We are building an application card based on i.MX 1050, about the SEMC interface, I saw it support SRAM in Chapter 49, but when I veiw the Signal, I can't see the pin of RD and WR. The pin of SEMC_WE, the description is like this "Write Enable (For SDRAM only)" which make me confused.I can't find other RD and WR singal to support the SRAM like IS62WV25616BLL-55TLI-TR.

     And I also can't find it on Pins Tool for i.MX.

     So, I wanted know if,

     1. My understanding is correct with respect to parallel bus interface.

     2. Is there any another way I can make it?

Thanks,

Zefeng Tao

Labels (1)
0 Kudos
Reply
3 Replies

896 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Taoze Feng,

But IS62WV25616BLL also hasn't RD and WR. Most current commercial SRAM hasn't these pins.

jingpan_0-1616059571416.png

MCUXpresso IDE has integrated pin config tool. If you use Keil/IAR, you can use MCUxpresso Config Tools to configure pins. It can be downloaded from

 https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-c...

 

Regards,

Jing

0 Kudos
Reply

876 Views
TaoZefeng
Contributor I

Hi, Jing  

    Thanks for your reply, we always used the IC like LY62256SL which had OE and WE.and now we want to use I.MX RT1050,and now I didn't know how to design to achieve this with parallel bus interface, so we now commucate with the IC using serial interface like spi.

     But I also want to know how to use the parallel interface, It means I should use the IC like the IS62WV25616BLL which without RD and WR,and I must match the sequence if I use the FPGA. Is it means I.MX RT1050 can't support the IC like LY62256SL. Sorry, I don't konw how the upload the pic.

     Now I had use the MCUxpresso Config Tools to configure pins and the keil to compile th project,thanks.

0 Kudos
Reply

865 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

SEMC doesn't support 8080 bus interface. Please use FlexIO to connect to LY62256SL. It can emulate 8080 bus interface.

 

Regards,

Jing

0 Kudos
Reply