Hi All,
I am using MIMXRT1052xxx6B controller in project with QSPI flash memory from 0x60001000 location.
I am not able to flash on to the board using jlink. It is running last loaded image and now not accepting the new image via jlink.
Please see the terminal it is running but code is not flashing on board.
When i am trying to erase using Jlink commander then i am getting
this error so please if any one is having any idea regarding this please let me know the solution for this.
Thanks in advance.
Thanks and Regards,
Shriram Madhavai
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I was wondering if you can introduce your testing environment, such as the board, demo code, etc.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------