MIMXRT1176CVM8A (MIMXRT1176 Family's): For possibility of using GPIO SNVS as normal GPIOs.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1176CVM8A (MIMXRT1176 Family's): For possibility of using GPIO SNVS as normal GPIOs.

ソリューションへジャンプ
267件の閲覧回数
Yogesh96
Contributor II

Hi Team,

We are using MIMXRT1176CVM8A in our design whose SNVS bank's GPIO are not Tamper pins. We are not connecting battery to VDD_SNVS_IN since we have separate battery backed up RTC interface to the controller.

We have connected 3.3V external supply to VDD_SNVS_IN. The output of the VDD_SNVS_ANA is 1.8V which is given to NVCC_SNVS supply. 

However, owing to GPIO shortage in our design, we are thinking of using the SNVS Bank's GPIO as normal GPIO pins. 

But if we connect the VDD_SNVS_ANA to NVCC_SNVS, then the max source/sink capability of the all the pins of SNVS bank comes to 1mA which is way below what we need.

 

Hence, we are thinking of connecting external VDD_1V8 to the NVCC_SNVS.

Can you please look into this and suggest if it can be done.? 

Our intention is to connect external 1.8V to NVCC_SNVS and make use of the SNVS Bank's GPIO to have higher current drive capability to drive the MOSFET drivers of LEDs

タグ(1)
0 件の賞賛
返信
1 解決策
224件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

The chip internal LDO VDD_SNVS_ANA should be tied together with NVCC_SNVS. I do not suggest using a configuration outside our recommendations.

Best regards,
Omar

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
225件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

The chip internal LDO VDD_SNVS_ANA should be tied together with NVCC_SNVS. I do not suggest using a configuration outside our recommendations.

Best regards,
Omar

0 件の賞賛
返信