MIMXRT1166D ADC is 1.8V max?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1166D ADC is 1.8V max?

ソリューションへジャンプ
1,239件の閲覧回数
maglash64
Contributor II

Hi, 

I am developing a custom board for MIMXRT1166D,

In the EVK schematic, the ADC_VREFH is attached to the 1V8 rail.

Is the max voltage on analog pins 1V8? If so then Why?

Because MIMXRT1050 and MIMXRT1060 had max ADC input voltage of 3V3.

We are interfaring with a 3V3 sensor that gives an analog output, thus this became an issue when

we began porting our product over MIMXRT1166.

Why did the max ADC voltage change from MIMXRT1050/60 to MIMXRT1160/70 ?

0 件の賞賛
返信
1 解決策
1,219件の閲覧回数
maglash64
Contributor II

After researching for a white, I found out in the reference manual that it is indeed possible to provide a voltage greater than VDD_ADC_VREFH (1.8V) on any of the ADC pins.

To do that one needs to set the CSCALE of the particular ADC which scales the input to the range of the specified ADC ( VREH to VREFL).

 

MIMXRT1166-ADC.jpg

 

 

MIMXRT1166-ADC2.jpg

 

元の投稿で解決策を見る

1 返信
1,220件の閲覧回数
maglash64
Contributor II

After researching for a white, I found out in the reference manual that it is indeed possible to provide a voltage greater than VDD_ADC_VREFH (1.8V) on any of the ADC pins.

To do that one needs to set the CSCALE of the particular ADC which scales the input to the range of the specified ADC ( VREH to VREFL).

 

MIMXRT1166-ADC.jpg

 

 

MIMXRT1166-ADC2.jpg