Hi all
Could you share the datasheet of J6 connector (302-1-10P-SMT-D, Junhao) ?
I'd like to make cables for debugging i.MXRT board, but I couldn't find the connector dimension information.
Is it same as 20021511-00010T1LF of Amphenol ICC?
解決済! 解決策の投稿を見る。
Hi @Eugene3 ,
Yes, any connector be connected as long as it meets the spec of 2x5pin & 50mil pitch connector can be used!
You even also can use the standard JTAG interface if you design your own RT1170 board, then you can use the JLINK as the debugger.
Wish it helps you!
Best Regards,
Kerry
Hi @Eugene3 ,
Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.
At first, just check with you, you are using the MCU LINK or the MCU LINK PRO?
or this one:
This one for J6?
If this one, it is 2*5, 50mil interface, you just need to find the related cable.
As I know, the MCU-LINK should contains this cable, you can't find it, right?
Wish it helps you!
Best Regards,
Kerry
Hi @kerryzhou
Thank you for your prompt replying.
I'll use MCU-Link Debug Probe, not Pro.
Actually I have not purchased the debugger yet, and I'm designing schematic of my application using RT1170. I'd like to use the same connector as the one on debugger in my application, but I couldn't find the connector spec.
I'm not familiar with SWD connector. Can any connector be connected as long as it meets the spec of 2x5pin & 50mil pitch connector?
Hi @Eugene3 ,
Yes, any connector be connected as long as it meets the spec of 2x5pin & 50mil pitch connector can be used!
You even also can use the standard JTAG interface if you design your own RT1170 board, then you can use the JLINK as the debugger.
Wish it helps you!
Best Regards,
Kerry
Thank you, I understand.