IMXRT1172 flashloader not starting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMXRT1172 flashloader not starting

跳至解决方案
1,521 次查看
Kaidou
Contributor II

Hello.

I'm working with a IMXRT1172 board. I enabled the Encrypted (OTFAD) authenticated secure boot and enabled the HAB and I was able to flash the board.

Then yesterday i tried again to flash a new image and now the flashloader is not starting.

I get the following error:


### Load FlashLoader ###
blhost -t 5000 -u 0x1FC9,0x013D -j -- load-image "..\secure_provisioning0\bootable_images\signed_MIMXRT1172_flashloader.bin"
{
"command": "load-image",
"response": [],
"status": {
"description": "0 (0x0) Success.",
"value": 0
}
}
blhost succeeded
### Waiting FlashLoader to be initialized for 5 seconds ###
### Timeout wait value can be adjusted from Preferences ###
### Check presence of FlashLoader ###
blhost -t 2000 -u 0x15A2,0x0073 -j -- get-property 7 0
ERROR:SPSDK: Selected 'usb' device not found.
blhost failed

 

The board is correctly connected and in serial downloader mode.
I tried with another board with secure boot not enabled and the connection works.

What might be the issue?

Thanks

标记 (3)
0 项奖励
回复
1 解答
1,288 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Kaidou 

If you selected the HAB closed life cycle there is no way to disable HAB or change keys, since they are already burned. 

 

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,362 次查看
Kaidou
Contributor II

Is it possible that the flashloader is signed with a different key than the SRK burnt into the board?

 

0 项奖励
回复
1,333 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Kaidou 

Per my understanding , when HAB is enabled, the flashloader must be signed with keys derived from the same CA that was used to sign the image.

Are you still using the same workspace and keys ? Do you have the same certificate?

Best regards, 

Diego

 

 

 

 

0 项奖励
回复
1,318 次查看
Kaidou
Contributor II

Thanks for your reply!

I'm guessing I don't have the correct keys anymore. Is there a way to recover the board somehow?
But I don't have much hope.

0 项奖励
回复
1,289 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Kaidou 

If you selected the HAB closed life cycle there is no way to disable HAB or change keys, since they are already burned. 

 

0 项奖励
回复
1,259 次查看
Kaidou
Contributor II

Ok!

Thank you very much for your help!

0 项奖励
回复