IMXRT106S - SAI3 MCLK configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT106S - SAI3 MCLK configuration

2,071 Views
jnj
Contributor III

Hi All,

I want to interface SAI3 in imxrt106s with an audio codec .Audio codec will be the slave and IMXRT106s will be the master. MCLK needed for the audio codec will be given by SAI3. What is the default MCLK value of SAI3 in sln-local2-iot sdk and how can we control the mclk frequency?I have configured GPIO_EMC_37 as MCLK(direction output) .While probing clock frequency,it is  showing as 12MHz. How can we confirm whether it is correct or not?

Please guide me to configure the mclk

Thanks in advance!

0 Kudos
Reply
11 Replies

2,061 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

Did you review the application notes, AN13208, AN13363, AN_RT1060_v1.5 [Audio performance requirements for Audio Front End of i.MX RT106A/L/S and i.MX RT105S] and AN13212 may be could help you, I will download the SDK for review if there is any more information.

Best regards,
Pavel

0 Kudos
Reply

2,046 Views
jnj
Contributor III

Hi @Pavel_Hernandez 

Thanks for the response.I will check the documents and also could you please review the sdk  ?

0 Kudos
Reply

2,040 Views
jnj
Contributor III

Hi @Pavel_Hernandez ,

I have checked all the above mentioned documents.But there is no explanation for mclk configuration in any of the above files.Could you please review the sln-lcal2-iot sdk ?

0 Kudos
Reply

2,036 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

Could you tell me if you are using the evaluation board o only have the MCU? I have already the SDK installed, Could you tell me the example you are based on?

Pavel_Hernandez_0-1658857474660.png

Best regards,
Pavel

0 Kudos
Reply

2,027 Views
jnj
Contributor III

Hi @Pavel_Hernandez ,

I am using only the MCU and working based on local_demo.

0 Kudos
Reply

1,986 Views
jnj
Contributor III

Hi @Pavel_Hernandez ,

 

Could you please update on this?

0 Kudos
Reply

1,968 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I'm following your case, sorry for the late response I was trying to get an SLN-LOCAL2 to test it, but I review the code and I compared it to other examples in the RT1064. 

I'm unavailable to find the code like this.

wm8960_config_t wm8960Config = {
    .i2cConfig = {.codecI2CInstance = BOARD_CODEC_I2C_INSTANCE, .codecI2CSourceClock = BOARD_CODEC_I2C_CLOCK_FREQ},
    .route     = kWM8960_RoutePlaybackandRecord,
    .leftInputSource  = kWM8960_InputDifferentialMicInput3,
    .rightInputSource = kWM8960_InputDifferentialMicInput2,
    .playSource       = kWM8960_PlaySourceDAC,
    .slaveAddress     = WM8960_I2C_ADDR,
    .bus              = kWM8960_BusI2S,
    .format = {.mclk_HZ = 6144000U, .sampleRate = kWM8960_AudioSampleRate16KHz, .bitWidth = kWM8960_AudioBitWidth16bit},
    .master_slave = false,
};
codec_config_t boardCodecConfig = {.codecDevType = kCODEC_WM8960, .codecDevConfig = &wm8960Config};

So let me get more information, I will ask to another team.

Best regards,
Pavel

0 Kudos
Reply

1,951 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

--> What is the default MCLK value of SAI3 in sln-local2-iot SDK 

Based on sln-local2-iot SDK, SAI3 CLK is provided by Audio/Video PLL CLK(786.48MHz)

And MCLK divider is 64, so the SAI3 MCLK is 768.48/64 = 12.28875MHz. Except for the MCLK, Need to check BCLK and sync clock.

--> How to configure MCLK

Example:

/*Clock setting for SAI3*/
CLOCK_SetMux(kCLOCK_Sai3Mux, BOARD_AMP_SAI_CLOCK_SOURCE_SELECT);
CLOCK_SetDiv(kCLOCK_Sai3PreDiv, BOARD_AMP_SAI_CLOCK_SOURCE_PRE_DIVIDER);
CLOCK_SetDiv(kCLOCK_Sai3Div, BOARD_AMP_SAI_CLOCK_SOURCE_DIVIDER);

BOARD_SAI_Enable_Mclk_Output(SAI3, true);

Best regards,
Pavel

0 Kudos
Reply

1,947 Views
jnj
Contributor III

Hi @Pavel_Hernandez ,

Thank you so much for the response.

So for changing the MCLK we need to change BOARD_AMP_SAI_CLOCK_SOURCE_DIVIDER and  BOARD_AMP_SAI_CLOCK_SOURCE_PRE_DIVIDER?

0 Kudos
Reply

1,939 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

I suggest modifying the macro [BOARD_AMP_SAI_CLOCK_SOURCE_DIVIDER] to change the result in Hz.

Best regards,
Pavel

0 Kudos
Reply

1,932 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

This is how the macro affects the MCLK.

MCLK = PLL audio clock / (BOARD_AMP_SAI_CLOCK_SOURCE_PRE_DIVIDER + 1) / (BOARD_AMP_SAI_CLOCK_SOURCE_DIVIDER + 1)

Best regards,
Pavel

0 Kudos
Reply