IMXRT1062 POR_B fails and stays pulled low

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1062 POR_B fails and stays pulled low

493 Views
odd_bikes
Contributor III

Hi,

We have this incredibly odd situation whereby the whole POR_B line gets pulled low. There's no real pattern, happens in maybe 0.5% of power-up cases for our product. The effect we notice is as shows in the screenshot attached, essentially even though the supervisor chip should pull the line high and allow the MCU to start, the line stays low. The real oddity is that, if we leave the product powered for anywhere between 5-60 minutes, it will recover and resume functioning as usual. 

There is one thing in the design which strays from the official EVK schematic: the pull-up for POR_B is to 3V3, while VDD_SNVS_IN is connected to 3V3 through a diode. But we don't use SNVS mode.

Labels (1)
0 Kudos
Reply
1 Reply

456 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Could you share some scopes of the POR_b along with the power sources? Ideally, the external IC should control the POR_b status at power-up so if it stays stuck the issue may be on the IC.

Best regards,
Omar

0 Kudos
Reply