FlashLoader don't work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlashLoader don't work

709 Views
eric_yp_chen
Contributor I

Hi 

I'm developing a ram project with rt1052. 

I just follow this guide to generate bootable image for SPI Nor flash but failed.

It stuck at "Section: 0x0" while generating bin file. 

   pastedImage_1.png

The command line as below:

elftosb.exe -f imx  -V -c ../../bd_file/imx10xx/imx-dtcm-unsigned.bd -o TEST_MCU.bin TEST.s19

This project was modified from usb  dev_vcom_bm sdk sample.

And I wish to make a boot flow as below:

1. Boot image storage in QSPI nor flash and connect to FlexSPI-A

2. The program/data will be copy from nor flash to SRAM-DTC then execute after power up

Here are my project information

pastedImage_2.png

pastedImage_4.png

pastedImage_5.png

pastedImage_1.png

I also tried using MCUbootUtility , it shown error message like this:

pastedImage_6.png

Labels (1)
0 Kudos
Reply
1 Reply

610 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Eric Chen,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you refer to the post: https://community.nxp.com/docs/DOC-341317 for details.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply