I am trying to use inputs GPIO_B0_12 and GPIO_B0_13 as phase inputs to the ENC peripheral.
In the SDK samples the phase pins have pull-down set, but I am trying to use an encoder with common to GND, so I need pull-up enabled. In the PIN CONFIG tool I have set pull-up for those pins, and I also tried using an external 10k pull-up resistor, but regardless it seems those pins have pull-down enabled.
Even just scoping the pin directly and using GPIO, I don't see the input pulled up... On other pins I have successfully set pull-up, but GPIO_B0 pins seem to all be pulled down.
Here is my pin setup:
Any help appreciated!
解決済! 解決策の投稿を見る。
Hi Jack
you are right, in general if GPIO_B0 pins should be used later for other purposes one can use
isolation circuit described in sect.2.3 Bus isolation circuit i.MX6 System Development User’s Guide
https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jack
you are right, in general if GPIO_B0 pins should be used later for other purposes one can use
isolation circuit described in sect.2.3 Bus isolation circuit i.MX6 System Development User’s Guide
https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Well, a lot of the GPIO_B0 pins are used at boot time for BOOT_CFG, so they have external 10k pull-downs (on the EVK).
So it doesn't look like you can use B0 as pull-up inputs while the fuses aren't set.