Concurrent Wi-Fi + Bluetooth with MCUXpresso SDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Concurrent Wi-Fi + Bluetooth with MCUXpresso SDK

1,108 次查看
veranith
Contributor I

Hello

Running Wi-Fi/Bluetooth (on a Cypress-based module like Murata type 1DX) with an i.MXRT1060 using MCUXpresso SDK :

I can find Wi-Fi or Bluetooth example projects on the SDK but :

- is there one that shall demonstrate a concurrent usage of Wi-Fi and Bluetooth ? 

If not, can somebody confirm me that this is feasible ? 

anticipation : is this (or will this be) possible with NXP-based modules like Panasonic PAN9026 ?

Many thanks

Veranith

0 项奖励
回复
2 回复数

1,044 次查看
romitchatterjee
Contributor V

<Removed>

0 项奖励
回复

1,093 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Veranith,

Have you checked the evkmimxrt1060_wiced_ble_4343W example? This demo configures the Wi-Fi driver to use STA mode and advertises via BLE.

Regarding your question about Panasonic module, unfortunately we do not have examples yet using WiFI + BLE and I do not have a date of when this will be available.

Best regards,

Felipe

0 项奖励
回复