Hi,sir
Requirements:
The system requires data interaction between RT1052 and IMX8, and the wider the rate, the better
What is the maximum bandwidth communication mode between imx8 and RT1052?
解決済! 解決策の投稿を見る。
The bandwidth will depend on the protocol used for communication.
You can opt to use LPSPI or ethernet for the communication between devices.
Best regards,
Omar
The bandwidth will depend on the protocol used for communication.
You can opt to use LPSPI or ethernet for the communication between devices.
Best regards,
Omar
The amount of data each interaction between the two chips is 512 bytes, and the less time spent, the better