Chipset comination of RT1052 + PN7150 for payment system

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Chipset comination of RT1052 + PN7150 for payment system

跳至解决方案
1,359 次查看
andy_kim
Contributor IV

Hello,

We've used RT1052 on our device.

and We're planning to add PN7150 for contactless payment system on it.

 

I wonder if that chipset combination is no problem for working as payment system.

Or  Shoule we use KL81 MCU + PN7150 for contactless payment system?

 

Thank you,

Andy

0 项奖励
回复
1 解答
1,345 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Andy,
Thanks for your reply.
1) Do you think RT1050 has a security risk when using it for a contactless payment solution?
-- Yes.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,352 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Shoule we use KL81 MCU + PN7150 for contactless payment system?
-- Benefit from the rich security features, I consider the KL81 is better choice than the RT1052.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,347 次查看
andy_kim
Contributor IV

Hi, Jeremyzhou

Thanks for your prompt reply and comments.

Actually, we just use NFC technology for contactless payment.

As far as I know, K81/KL81 is a solution for POS teminal which supports contact card, contactless card and magstripe card for payment.

Do you think RT1050 have a security risk when using it for contactless payment solution?

 

Thank you

Andy

0 项奖励
回复
1,346 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Andy,
Thanks for your reply.
1) Do you think RT1050 has a security risk when using it for a contactless payment solution?
-- Yes.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,325 次查看
andy_kim
Contributor IV

Hi, Jeremyzhou,

 

Thanks for your reply.

 

Let me close this case

 

Thank you,

Andy

0 项奖励
回复