Chipset comination of RT1052 + PN7150 for payment system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Chipset comination of RT1052 + PN7150 for payment system

Jump to solution
1,360 Views
andy_kim
Contributor IV

Hello,

We've used RT1052 on our device.

and We're planning to add PN7150 for contactless payment system on it.

 

I wonder if that chipset combination is no problem for working as payment system.

Or  Shoule we use KL81 MCU + PN7150 for contactless payment system?

 

Thank you,

Andy

0 Kudos
Reply
1 Solution
1,346 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Andy,
Thanks for your reply.
1) Do you think RT1050 has a security risk when using it for a contactless payment solution?
-- Yes.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
1,353 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Shoule we use KL81 MCU + PN7150 for contactless payment system?
-- Benefit from the rich security features, I consider the KL81 is better choice than the RT1052.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,348 Views
andy_kim
Contributor IV

Hi, Jeremyzhou

Thanks for your prompt reply and comments.

Actually, we just use NFC technology for contactless payment.

As far as I know, K81/KL81 is a solution for POS teminal which supports contact card, contactless card and magstripe card for payment.

Do you think RT1050 have a security risk when using it for contactless payment solution?

 

Thank you

Andy

0 Kudos
Reply
1,347 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Andy,
Thanks for your reply.
1) Do you think RT1050 has a security risk when using it for a contactless payment solution?
-- Yes.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,326 Views
andy_kim
Contributor IV

Hi, Jeremyzhou,

 

Thanks for your reply.

 

Let me close this case

 

Thank you,

Andy

0 Kudos
Reply