Can VBB_USB_CAP pin be floating?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can VBB_USB_CAP pin be floating?

Jump to solution
1,254 Views
giuseppescarpi
Contributor III

Hi fellow engineers,

the board I'm working has very limited room available. I plan NOT to use USB, so the question is: can I leave VDD_USB_CAP floating?

Thanks

Giuseppe

Labels (1)
0 Kudos
Reply
1 Solution
1,247 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @giuseppescarpi,

You can keep USB pins floating. If  USB VBUS is not applied, there is no need to connect the VDD_USB_CAP.

Best Regards,

Alexis Andalon

View solution in original post

1 Reply
1,248 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @giuseppescarpi,

You can keep USB pins floating. If  USB VBUS is not applied, there is no need to connect the VDD_USB_CAP.

Best Regards,

Alexis Andalon