Hi,
I am using IMXRT1064 in my new project. I want to execute the code from internal flash(in datasheet written as 4MB internal flash is available). Is there any setting in the complier to load the code into internal flash. I dont want to use any external memory option. Please help me out
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there any setting in the complier to load the code into internal flash. I dont want to use any external memory option. Please help me out
-- Actually, it doesn't need any extra setting to load the code into the internal flash, to provide the fastest possible support, I'd highly recommend you to refer to the guide.
Have a great day.
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------