Hi,
I want to implement Secure boot on RT1062 (or RT1021).
However, it seems that no such example is provided in the SDK.
I've already looked at the Security Reference Manual.
Is there any place where a well-implemented example is provided?
Thanks.
Hi Joseph,
I highly recommend you to refer to the following application note:
https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=AN12681&appType=moderated
Additionally, there is a step by step training material that could be helpful for you.
Secure Boot on the i.MX RT10xx Crossover MCUs | NXP Semiconductors
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------